WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

Through the company's strategic direction for its business model, WEG has, in all its business units, more efficient solutions and products with less environmental impact, such as renewable energy (solar and wind power), electric mobility and energy efficiency. WEG develops products considering strict risk criteria related to health and safety. In the development phase, analyzes such as Quality Function Deployment (QFD) and Risk Assessment are applied.

Below are some highlights, considering the variety of products and solutions that the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solar Power

WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.

Hydroelectric Generation

WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.

São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.

Commercial and Industrial Energy Storage

Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.

Transformers for Renewable Energy

The reliability of the transformers developed for solar plants aims at guaranteeing the supply of energy, allowing access to electricity through renewable energy generation sources. In the line of transformers for wind farms, WEG developed an extremely compact electrical and mechanical transformer design. Additionally, due to the installation layout, in which the source and the transforming unit are very close to each other, the system produces smaller losses and greater energy efficiency.

Mobilidade Elétrica

Soluções integradas para veículos elétricos

A WEG desenvolve continuamente tecnologias inovadoras para criar sistemas de tração elétrica, bem como toda a infraestrutura elétrica necessária para operação de veículos elétricos. Os sistemas de tração elétrica WEG podem ser aplicados em diversos veículos rodoviários, ferroviários e de navegação, tais como caminhões e ônibus urbanos, furgões, empilhadeiras elétricas, trens, monotrilhos, navios de suporte e rebocadores.

Soluções Digitais

Sistemas inteligentes e sustentáveis

Sistemas inteligentes são capazes de integrar os mais variados dispositivos e máquinas, bem como instalações e processos, promovendo eficiência na tomada de decisão e aumento da eficiência operacional. Soluções e sistemas mais inteligentes também promovem a utilização mais eficiente de recursos energéticos ajudando a reduzir pegada de carbono das operações em todos os níveis.

Sistemas de Automação

A WEG fornece sistemas de controle completamente integrados, garantindo ainda alto desempenho dos processos industriais, facilidade de operação e ganho de produtividade por meio de tecnologia de ponta. O sucesso da integração desse sistema está na sinergia dos produtos WEG, na qual motores, drives, geradores, painéis elétricos e softwares são integrados, fornecendo a solução ideal para cada necessidade. O controle de processos industriais exige sistemas de automação com elevado grau de confiabilidade e disponibilidade, além de facilidade para equipes de manutenção no gerenciamento de ativos, estendendo a vida dos equipamentos e racionalizando o uso de recursos.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

O WEG Transformer Fleet Management é a solução ideal para monitorar on-line e gerir a frota de transformadores a óleo ou do tipo seco, possibilitando que os clientes maximizem a eficiência das suas operações, em apoio à gestão otimizada de plantas industriais, de geração de energias renováveis e de infraestrutura. Já a solução WEG Power Transformer Specialist é uma solução digital aplicada no monitoramento e na gestão de transformadores de potência que, integrada à plataforma WEG Transformer Fleet Management, centraliza os sinais de uma série de sensores instalados no equipamento.

WEG Motion Fleet Management

Desenvolvido para levar mais praticidade e agilidade na operação, na manutenção e na gestão de plantas industriais, o WEG Motion Fleet Management é a solução ideal para monitorar e elevar a disponibilidade da frota de acionamento industrial. Baseado em tecnologia “cloud computing”, o monitoramento dos ativos pode ser acompanhado a qualquer momento e de qualquer parte do mundo. Com o Motion Fleet Management, é possível conhecer o estado operacional de motores e drives (inversores e soft-starters) de baixa e média tensão, redutores, motorredutores, compressores entre outros ativos, que estejam aplicados em qualquer tipo de indústria ou instalação

Tenologia Ultra Low Bake (ULB) para Tintas

A tecnologia Ultra Low Bake (ULB) consiste em reduzir o tempo de cura ou a temperatura de cura das tintas em pó. Atrelado a essa redução de tempo ou temperatura (que pode chegar até 35% de redução), reduzindo a quantidade de gás que é utilizado nas estufas de cura dos seus clientes e parceiros e reduzindo as emissões de GEE.

Os parceiros da WEG que possuem essa tecnologia na sua linha de produção, além da redução do impacto ambiental, têm aumento significativo de produtividade e em sua competitividade. A WEG possui quarenta produtos desenvolvidos com essa finalidade.

Eficiência material e avaliação ambiental do produto

A WEG adota, em sua cadeia de valor, iniciativas que estão alinhadas aos princípios da economia circular, através de práticas como reinserção de resíduos dos processos como matérias-primas, como por exemplo sucatas de aço da estamparia para fabricação de peças fundidas, adoção de programas de recuperação de materiais no fim do ciclo de vida de produtos através da logística reversa e planos de troca.

A aplicação desses conceitos e práticas permitiram à WEG atingir um índice de eficiência material próximo de 85%. A WEG também está em constante melhoria e evolução da eficiência energética de seus produtos e de soluções de retrofit para a extensão da vida útil de algumas linhas de produtos. Equipes qualificadas atuam tanto nos processos de desenvolvimento de novos produtos e na concepção de novas linhas quanto na implantação de processos industriais mais eficientes.

A WEG aplica a ACV (Análise de Ciclo de Vida), gerando os EPDs (Environmental Product Declarations) conforme as demandas dos clientes, pretendendo, nos próximos anos, ampliar a aplicação dessas ferramentas.

Saiba mais sobre as ações da WEG em Sustentabilidade

Hotel & SPA beira-mar na região nordeste do Brasil será alimentado por transformador a seco encapsulado WEG

Hotel & SPA beira-mar na região nordeste do Brasil será alimentado por transformador a seco encapsulado WEG

Referência em eficiência energética e confiabilidade, o transformador seco é a escolha ideal para aplicações no segmento de infraestrutura

WEG divulga Relatório Anual Integrado, reforçando compromissos com a sustentabilidade

WEG divulga Relatório Anual Integrado, reforçando compromissos com a sustentabilidade

Companhia apresenta avanços significativos em diversos aspectos

WEG fornece hidrogeradores para projeto em Portugal

WEG fornece hidrogeradores para projeto em Portugal

Os hidrogeradores irão fortalecer a produção de energia renovável na central hidrelétrica

WEG impulsiona o Projeto Sucuriú, primeira fábrica de celulose branqueada da Arauco no Brasil

WEG impulsiona o Projeto Sucuriú, primeira fábrica de celulose branqueada da Arauco no Brasil

Soluções tecnológicas da WEG reforçam eficiência, confiabilidade e sustentabilidade no setor de celulose

WEG atinge dois mil geradores fornecidos ao cliente Vestas do Brasil Energia Eólica

WEG atinge dois mil geradores fornecidos ao cliente Vestas do Brasil Energia Eólica

Marco que reforça a parceria sólida e compromisso com a energia renovável

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability