The circular economy seeks to maximize the value of resources while minimizing waste and environmental impacts. In this model, products are designed to be durable, repairable and recyclable, encouraging the reuse and recycling of materials. Instead of following the traditional linear model of production and consumption, in which products are manufactured, used and discarded, the circular economy promotes the idea of a continuous cycle, where materials are kept in use for as long as possible.
This approach not only contributes to the conservation of natural resources but also stimulates innovation, job creation and sustainable economic growth, making it essential to address today's global challenges such as climate change and resource scarcity.
Consolidating WEG's commitment, we have ISO 14,001 certifications demonstrating environmental management in the company's operations.
WEG operations have a selective waste collection system. In this way, residues are separated and sent to recyclers of each material, enabling their appreciation and the reintroduction of such materials in different production cycles. It is important to emphasize that part of the waste generated in the operations is recycled by WEG itself, returning to the process and forming part of its products. All waste is sent to environmentally responsible companies, selected and developed by WEG's environmental management team.
WEG has had an Energy Efficiency Policy since 2012, showing its commitment to the management of this input. This policy is deployed into actions to monitor and reduce energy consumption, which contributes to improving the environment. WEG intends to increasingly make its energy sources cleaner, renewable and sustainable.
WEG monitors the water consumption of its operations and has several operational controls that ensure efficient management of this resource, thus avoiding waste and promoting conscious consumption. All effluents generated in operations are properly treated and periodically monitored in order to ensure compliance with legislation and minimize impacts on different stakeholders.
Part of the effluents treated in the operations are reused in the internal processes, where some effluent treatment plants enable the reuse of up to 100% of the treated effluent. We have adopted initiatives focused on reducing water consumption and effluent generation by controlling leaks, monitoring consumption and counting on the support of programs that engage all employees in this objective, such as KaizenWEG and WEG Manufacturing System.
Les investissements environnementaux sont caractérisés en trois catégories :
Nous possédons une usine d'emballage, RF Reflorestadora, au Brésil. Cette unité produit tous les emballages en bois utilisés dans nos différentes gammes de produits. À cette fin, nous disposons de nos propres zones de reforestation qui garantissent l'approvisionnement continu en bois et la préservation de cette ressource naturelle, ainsi que de zones de forêts naturelles, de réserves légales et d'aires de préservation permanente qui contribuent à la préservation de la biodiversité locale.
Les zones respectent toute la législation et les exigences légales, y compris une zone de conservation des forêts natives beaucoup plus importante que le minimum établi pour la réserve légale.
En outre, WEG encourage et soutient les initiatives de reforestation consciente et de conservation de la nature, et investit dans le boisement de ses parcs industriels.
KaizenWEG est l'une des formes de management participatif de WEG, où tous les employés sont encouragés à promouvoir des améliorations dans leur environnement de travail ou dans d'autres domaines de l'entreprise, en identifiant les gaspillages, en analysant les causes et en participant aux équipes de mise en œuvre des améliorations.
La recherche collective de l'excellence opérationnelle et de la durabilité dans un contexte de verticalisation des processus fait du management participatif un élément clé de l'amélioration des résultats de WEG.
Le système de gestion de l'amélioration continue de WEG est le WMS, dont l'objectif principal est d'identifier et d'éliminer les pertes et le gaspillage.
Les résultats sont maximisés grâce à des matrices de priorisation de la sécurité, de la qualité, des coûts et des émissions de GES (gaz à effet de serre), qui guident le développement de projets visant à optimiser ou éliminer ces gaspillages, contribuant ainsi à un monde plus efficace et plus durable.
En plus des fronts de travail d'optimisation, des équipes multidisciplinaires agissent comme des points centraux d'amélioration continue, apportant des innovations et des ruptures dans nos processus.
L'un de ces points centraux est le pilier Environnement et Energie, qui vise et systématise la réduction des impacts environnementaux, en travaillant à réduire ou éliminer la génération de déchets et d'émissions, la consommation de ressources énergétiques, le nettoyage chimique et les intrants en général.
Le recyclage est un sujet sérieux pour WEG, s'étendant jusqu'aux activités commerciales. Grâce au programme de réutilisation des moteurs électriques, le "Plan d'Échange", l'entreprise accorde une réduction à l'achat d'un nouveau moteur dont les performances dépassent les exigences légales en échange d'un moteur usagé. Outre l'avantage financier pour les clients, l'initiative garantit que le moteur à faible rendement n'est plus utilisé. Une fois collectés par l'entreprise, les moteurs sont démantelés et séparés en pièces pour être distribués à des recycleurs agréés et suivis.
Réduction de la consommation d'énergie électrique
Fiabilité de l'usine
Réduction des coûts opérationnels
Garantie d'usine
Produits standard - offrent une interchangeabilité complète avec les moteurs déjà installés
Article | 2019 | 2020 | 2021 | 2022 |
Produits vendus pouvant être réutilisés ou recyclés* (%) - Sur la base du poids | 65 | 66 | 68 | 73 |
Produits réellement réutilisés ou recyclés par l'entreprise* (%) - Sur la base du poids | 21 | 13 | 8 | 5 |
*Pourcentage basé sur le poids des produits vendus au cours de l'année.
Les investissements environnementaux sont classés en trois catégories :
Contrôle environnemental : Relatif au traitement et à l'élimination des déchets, au traitement des émissions atmosphériques et liquides, aux assurances responsabilité environnementale et à l'amortissement des appareils ainsi qu'aux dépenses liées aux matériaux et à la maintenance.
Équipement : Relatif à l'achat d'équipement pour le contrôle environnemental.
Gestion : Relatif à la rémunération du personnel de formation travaillant dans la gestion environnementale, à la recherche et au développement, ainsi qu'à la certification des systèmes de gestion environnementale.
Voici le montant investi dans chaque catégorie au Brésil.
Investissement | 2021 | 2021 | 2022 | 2022 |
Contrôles Environnementaux | 8.678 | 54,19 | 10.234 | 52,4 |
Équipement | 1.329 | 8,30 | 1.788 | 9,2 |
Gestion | 6.006 | 37,51 | 7.519 | 38,5 |
TOTAL | 16.013 | 100 | 19.540 | 100 |
En 2022, en tenant compte du personnel, 77 % du groupe WEG étaient couverts par la certification ISO 14001.
Cliquez ici pour accéder aux certificats
WEG dispose d'un processus de cycle d'audit environnemental qui couvre toutes ses opérations industrielles.
Dans le cadre de son processus d'audit environnemental annuel, WEG garantit le respect de la législation environnementale dans toutes ses opérations industrielles.
En 2023, la portée des unités surveillées a été étendue, incluant les adresses professionnelles de l'entreprise. Ainsi, 100 % des adresses mondiales de WEG sont maintenant incluses dans les indicateurs.
WEG dispose d'un système de collecte sélective des déchets dans ses opérations. Les déchets sont séparés et envoyés à des recycleurs, permettant ainsi leur récupération et la réintroduction de matériaux dans les cycles de production les plus divers. Une partie des déchets générés dans les opérations est également recyclée par WEG elle-même, revenant ainsi dans le processus et faisant partie de nos produits.
Article | Unité | 2019 | 2020 | 2021 | 2022 |
Total des déchets dangereux recyclés/réutilisés | Tonnes métriques | 0 | 0 | 0 | 0 |
Total des déchets dangereux éliminés | Tonnes métriques | 5 822 | 4 905 | 5 484 | 6 511 |
Déchets dangereux mis en décharge | Tonnes métriques | 1 266 | 1 338 | 1 138 | 850 |
Déchets dangereux incinérés avec récupération d'énergie | Tonnes métriques | 0 | 0 | 0 | 0 |
Déchets dangereux incinérés sans récupération d'énergie | Tonnes métriques | 4 556 | 3 567 | 4 346 | 5 661 |
Déchets dangereux avec méthode d'élimination inconnue | Tonnes métriques | 0 | 0 | 0 | 0 |
Couverture des données (en % du dénominateur) | % employés | 100 | 100 | 100 | 100 |
WEG a une politique d'efficacité énergétique depuis 2012, où elle montre son engagement envers la gestion de cette ressource. Cette politique développe des actions pour surveiller et réduire la consommation d'énergie, ce qui contribue à améliorer l'environnement. WEG a l'intention de rendre de plus en plus propres, renouvelables et durables ses sources d'énergie.
Consommation totale d'énergie | Unité | 2019 | 2020 | 2021 | 2022 |
Consommation totale d'énergie non renouvelable | MWh | 466,737 | 462,976 | 499,355 | 478,872 |
Consommation totale d'énergie renouvelable | MWh | 0 | 0 | 56,000 | 86,918 |
Consommation totale d'énergie (non renouvelable + renouvelable) | MWh | 466,737 | 462,976 | 555,355 | 565,790 |
Couverture des données (% du dénominateur) | pourcentage d'employés | 100 | 100 | 100 | 100 |
En 2022, WEG a assuré que 14 % de la consommation d'énergie provenait de sources renouvelables en achetant des certificats d'énergie renouvelable (I-REC) et des contrats bilatéraux.
En 2024, WEG aura environ 90 % de la consommation d'électricité du Brésil provenant de sources renouvelables, soit une moyenne de 45 MW.
WEG surveille les émissions atmosphériques liées aux composés organiques volatils. Voici le résultat des émissions liées aux équipements surveillés au cours des dernières années.
Article | 2019 | 2020 | 2021 | 2022 |
Émissions de composés organiques volatils - COV (t/an) | 93,5 | 135,2 | 114,5 | 139,3 |
Taux de couverture (%) | 56 | 56 | 56 | 61 |
Une des priorités principales de WEG est le respect de la législation environnementale applicable à ses opérations. Au cours des 3 dernières années, il n'y a eu aucune preuve d'amendes environnementales appliquées aux activités de WEG.