WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability

Eco-efficiency and Waste and Emission Management

Circular and efficient operations

The circular economy seeks to maximize the value of resources while minimizing waste and environmental impacts. In this model, products are designed to be durable, repairable and recyclable, encouraging the reuse and recycling of materials. Instead of following the traditional linear model of production and consumption, in which products are manufactured, used and discarded, the circular economy promotes the idea of a continuous cycle, where materials are kept in use for as long as possible.

This approach not only contributes to the conservation of natural resources but also stimulates innovation, job creation and sustainable economic growth, making it essential to address today's global challenges such as climate change and resource scarcity.

Consolidating WEG's commitment, we have ISO 14,001 certifications demonstrating environmental management in the company's operations.

Programs & Practices

Residues and energy

Solid residues

WEG operations have a selective waste collection system. In this way, residues are separated and sent to recyclers of each material, enabling their appreciation and the reintroduction of such materials in different production cycles. It is important to emphasize that part of the waste generated in the operations is recycled by WEG itself, returning to the process and forming part of its products. All waste is sent to environmentally responsible companies, selected and developed by WEG's environmental management team.

See more

 

Energy

WEG has had an Energy Efficiency Policy since 2012, showing its commitment to the management of this input. This policy is deployed into actions to monitor and reduce energy consumption, which contributes to improving the environment. WEG intends to increasingly make its energy sources cleaner, renewable and sustainable.

Water, effluents and water resources

WEG monitors the water consumption of its operations and has several operational controls that ensure efficient management of this resource, thus avoiding waste and promoting conscious consumption. All effluents generated in operations are properly treated and periodically monitored in order to ensure compliance with legislation and minimize impacts on different stakeholders.

 

Part of the effluents treated in the operations are reused in the internal processes, where some effluent treatment plants enable the reuse of up to 100% of the treated effluent. We have adopted initiatives focused on reducing water consumption and effluent generation by controlling leaks, monitoring consumption and counting on the support of programs that engage all employees in this objective, such as KaizenWEG and WEG Manufacturing System.

 

Investments and expenses in the environment

Environmental investments fall into three categories:

  • Environmental control: related to treatment and disposal of residues, treatment of atmospheric and liquid emissions, environmental liability insurances, depreciation of devices and expenses with materials and maintenance.
  • Equipment: related to the purchase of equipment for environmental control.
  • Management: related to the remuneration of training staff who act in environmental management, research and development, and certification of environmental management systems.

Emballages durables et préservation de la biodiversité

Nous possédons une usine d'emballage, RF Reflorestadora, au Brésil. Cette unité produit tous les emballages en bois utilisés dans nos différentes gammes de produits. À cette fin, nous disposons de nos propres zones de reforestation qui garantissent l'approvisionnement continu en bois et la préservation de cette ressource naturelle, ainsi que de zones de forêts naturelles, de réserves légales et d'aires de préservation permanente qui contribuent à la préservation de la biodiversité locale.

Les zones respectent toute la législation et les exigences légales, y compris une zone de conservation des forêts natives beaucoup plus importante que le minimum établi pour la réserve légale.

En outre, WEG encourage et soutient les initiatives de reforestation consciente et de conservation de la nature, et investit dans le boisement de ses parcs industriels.

Kaizen WEG

KaizenWEG est l'une des formes de management participatif de WEG, où tous les employés sont encouragés à promouvoir des améliorations dans leur environnement de travail ou dans d'autres domaines de l'entreprise, en identifiant les gaspillages, en analysant les causes et en participant aux équipes de mise en œuvre des améliorations.

La recherche collective de l'excellence opérationnelle et de la durabilité dans un contexte de verticalisation des processus fait du management participatif un élément clé de l'amélioration des résultats de WEG.

Moyenne sur la période 2019-2021: 1.144

WMS

Le système de gestion de l'amélioration continue de WEG est le WMS, dont l'objectif principal est d'identifier et d'éliminer les pertes et le gaspillage.

Les résultats sont maximisés grâce à des matrices de priorisation de la sécurité, de la qualité, des coûts et des émissions de GES (gaz à effet de serre), qui guident le développement de projets visant à optimiser ou éliminer ces gaspillages, contribuant ainsi à un monde plus efficace et plus durable.

En plus des fronts de travail d'optimisation, des équipes multidisciplinaires agissent comme des points centraux d'amélioration continue, apportant des innovations et des ruptures dans nos processus.

L'un de ces points centraux est le pilier Environnement et Energie, qui vise et systématise la réduction des impacts environnementaux, en travaillant à réduire ou éliminer la génération de déchets et d'émissions, la consommation de ressources énergétiques, le nettoyage chimique et les intrants en général.

En Savoir Plus

 

Plan de Remplacement WEG (Disponible uniquement au Brésil)

Le recyclage est un sujet sérieux pour WEG, s'étendant jusqu'aux activités commerciales. Grâce au programme de réutilisation des moteurs électriques, le "Plan d'Échange", l'entreprise accorde une réduction à l'achat d'un nouveau moteur dont les performances dépassent les exigences légales en échange d'un moteur usagé. Outre l'avantage financier pour les clients, l'initiative garantit que le moteur à faible rendement n'est plus utilisé. Une fois collectés par l'entreprise, les moteurs sont démantelés et séparés en pièces pour être distribués à des recycleurs agréés et suivis.

 

Avantages

  • Réduction de la consommation d'énergie électrique

  • Fiabilité de l'usine

  • Réduction des coûts opérationnels

  • Garantie d'usine

  • Produits standard - offrent une interchangeabilité complète avec les moteurs déjà installés

 

Article

2019

2020

2021

2022

Produits vendus pouvant être réutilisés ou recyclés* (%) - Sur la base du poids

65

66

68

73

Produits réellement réutilisés ou recyclés par l'entreprise* (%) - Sur la base du poids

21

13

8

5

 

*Pourcentage basé sur le poids des produits vendus au cours de l'année.

 

Investissements dans l'Environnement

Les investissements environnementaux sont classés en trois catégories :

Contrôle environnemental : Relatif au traitement et à l'élimination des déchets, au traitement des émissions atmosphériques et liquides, aux assurances responsabilité environnementale et à l'amortissement des appareils ainsi qu'aux dépenses liées aux matériaux et à la maintenance.

Équipement : Relatif à l'achat d'équipement pour le contrôle environnemental.

Gestion : Relatif à la rémunération du personnel de formation travaillant dans la gestion environnementale, à la recherche et au développement, ainsi qu'à la certification des systèmes de gestion environnementale.

Voici le montant investi dans chaque catégorie au Brésil.

Investissement

2021
Valeur 
(R$ Millier)

2021
(%)

2022
Valeur 
(R$ Millier)

2022
(%)

Contrôles Environnementaux

8.678

54,19

10.234

52,4

Équipement

1.329

8,30

1.788

9,2

Gestion  6.006 37,51 7.519 38,5
 TOTAL 16.013 100 19.540 100

 

 

Certification Environnementale

En 2022, en tenant compte du personnel, 77 % du groupe WEG étaient couverts par la certification ISO 14001.

Cliquez ici pour accéder aux certificats

 

Audits environnementaux

WEG dispose d'un processus de cycle d'audit environnemental qui couvre toutes ses opérations industrielles.

Dans le cadre de son processus d'audit environnemental annuel, WEG garantit le respect de la législation environnementale dans toutes ses opérations industrielles.

 

Indicateurs de performance

En 2023, la portée des unités surveillées a été étendue, incluant les adresses professionnelles de l'entreprise. Ainsi, 100 % des adresses mondiales de WEG sont maintenant incluses dans les indicateurs.

Déchets Solides

WEG dispose d'un système de collecte sélective des déchets dans ses opérations. Les déchets sont séparés et envoyés à des recycleurs, permettant ainsi leur récupération et la réintroduction de matériaux dans les cycles de production les plus divers. Une partie des déchets générés dans les opérations est également recyclée par WEG elle-même, revenant ainsi dans le processus et faisant partie de nos produits.

Article

Unité

2019

2020

2021

2022

Total des déchets dangereux recyclés/réutilisés

Tonnes métriques 

0 0 0

0

Total des déchets dangereux éliminés

Tonnes métriques  5 822

4 905

5 484 

6 511

Déchets dangereux mis en décharge

Tonnes métriques 1 266

1 338

1 138

850

Déchets dangereux incinérés avec récupération d'énergie

Tonnes métriques 0  0 0 0
Déchets dangereux incinérés sans récupération d'énergie Tonnes métriques 4 556  3 567 4 346 5 661

Déchets dangereux avec méthode d'élimination inconnue

Tonnes métriques 0  0 0 0

Couverture des données (en % du dénominateur)

% employés  100 100 100 100

 

Énergie

WEG a une politique d'efficacité énergétique depuis 2012, où elle montre son engagement envers la gestion de cette ressource. Cette politique développe des actions pour surveiller et réduire la consommation d'énergie, ce qui contribue à améliorer l'environnement. WEG a l'intention de rendre de plus en plus propres, renouvelables et durables ses sources d'énergie.

Consommation totale d'énergie

Unité

2019

2020

2021

2022

Consommation totale d'énergie non renouvelable

MWh

466,737 462,976 499,355

478,872

Consommation totale d'énergie renouvelable

MWh 0

0

56,000

86,918

Consommation totale d'énergie (non renouvelable + renouvelable)

MWh 466,737

462,976

555,355

565,790

Couverture des données (% du dénominateur)

pourcentage d'employés

100 100 100 100

Acquisition d'énergie renouvelable

En 2022, WEG a assuré que 14 % de la consommation d'énergie provenait de sources renouvelables en achetant des certificats d'énergie renouvelable (I-REC) et des contrats bilatéraux.

En 2024, WEG aura environ 90 % de la consommation d'électricité du Brésil provenant de sources renouvelables, soit une moyenne de 45 MW.

 

Émissions atmosphériques

WEG surveille les émissions atmosphériques liées aux composés organiques volatils. Voici le résultat des émissions liées aux équipements surveillés au cours des dernières années.

Article

2019

2020

2021

2022

Émissions de composés organiques volatils - COV (t/an)

93,5 135,2 114,5

139,3

Taux de couverture (%)

56

56

56

61

 

Infractions environnementales

Une des priorités principales de WEG est le respect de la législation environnementale applicable à ses opérations. Au cours des 3 dernières années, il n'y a eu aucune preuve d'amendes environnementales appliquées aux activités de WEG.

 

En savoir plus sur nos actions en durabilité

Seaside Hotel & SPA in Northeastern Brazil to Be Powered by WEG Encapsulated Dry-Type Transformer

Seaside Hotel & SPA in Northeastern Brazil to Be Powered by WEG Encapsulated Dry-Type Transformer

Renowned for its energy efficiency and reliability, the dry-type transformer is the ideal choice for infrastructure applications

WEG releases Integrated Annual Report, reinforcing its commitment to sustainability

WEG releases Integrated Annual Report, reinforcing its commitment to sustainability

Company reports significant progress across multiple areas

WEG supplies hydrogenerators for project in Portugal

WEG supplies hydrogenerators for project in Portugal

The hydrogenerators will strengthen renewable energy production at the hydroelectric power plant

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG's technological solutions enhance efficiency, reliability, and sustainability in the pulp sector

WEG reaches two thousand generators supplied to Vestas in Brazil

WEG reaches two thousand generators supplied to Vestas in Brazil

A milestone that reinforces a strong partnership and commitment to renewable energy

Groupe WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Téléphone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability