Through the company's strategic direction for its business model, WEG has, in all its business units, more efficient solutions and products with less environmental impact, such as renewable energy (solar and wind power), electric mobility and energy efficiency. WEG develops products considering strict risk criteria related to health and safety. In the development phase, analyzes such as Quality Function Deployment (QFD) and Risk Assessment are applied.
Below are some highlights, considering the variety of products and solutions that the company provides to the market through its different business units.
Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.
High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.
For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.
In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.
WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.
WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.
São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.
Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.
The reliability of the transformers developed for solar plants aims at guaranteeing the supply of energy, allowing access to electricity through renewable energy generation sources. In the line of transformers for wind farms, WEG developed an extremely compact electrical and mechanical transformer design. Additionally, due to the installation layout, in which the source and the transforming unit are very close to each other, the system produces smaller losses and greater energy efficiency.
WEG continually develops innovative technologies to create electric traction systems, as well as all the electrical infrastructure necessary for the operation of electric vehicles. WEG electric traction systems can drive various road, rail and navigation vehicles, such as urban trucks and buses, vans, forklifts, trains, monorails, support vessels and tugboats.
Smart systems are able to integrate different devices and machines, as well as installations and processes, promoting efficiency in decision-making and increasing operational efficiency. Smarter solutions and systems also promote more efficient use of energy resources helping reduce the carbon footprint of operations at all levels.
WEG supplies completely integrated control systems that guarantee high performance of industrial processes, easy operation and productivity gains by means of state-of-the-art technology. The success of the integration of this system is in the synergy of WEG products, where motors, drives, generators, electric panels and software applications are integrated, providing the ideal solution for each requirement. The control of industrial processes requires automation systems with high reliability and uptime levels, in addition to easy asset management by the maintenance teams, extending the equipment service life and streamlining the use of resources.
WEG Transformer Fleet Management is the ideal solution to monitor online and manage the fleet of oil or dry-type transformers, enabling customers to maximize the efficiency of their operations, supporting the streamlined management of industrial plants, renewable energy generation and infrastructure. WEG Power Transformer Specialist is a digital solution used to monitor and manage power transformers that, integrated with the WEG Transformer Fleet Management platform, centralizes the signals from several sensors installed on the equipment.
Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.
The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.
WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.WEG adopta, en su cadena de valor, iniciativas que están alineadas a los principios de la economía circular, a través de prácticas como reinserción de residuos de los procesos como materias primas, como por ejemplo chatarra de acero de la estampería, para fabricación de piezas fundidas, adopción de programas de recuperación de materiales en el fin del ciclo de vida de productos, a través de la logística reversa y de planes de cambio.
La aplicación de esos conceptos y prácticas permitieron a WEG alcanzar un índice de eficiencia material de cerca de 85%. WEG también está en constante mejora y evolución de la eficiencia energética de sus productos y de soluciones de retrofit para la extensión de la vida útil de algunas líneas de productos. Equipos cualificados actúan tanto en los procesos de desarrollo de nuevos productos y en la concepción de nuevas líneas, como en la implantación de procesos industriales más eficientes.
WEG aplica el ACV (Análisis de Ciclo de Vida), generando los EPDs (Environmental Product Declarations) conforme las demandas de los clientes, con el objetivo, en los próximos años, de ampliar la aplicación de esas herramientas.