WEG
  • Início
  • Produtos
    • PRODUTOS E SOLUÇÕES SUSTENTÁVEIS
    • Tecnologias e Inovação para a Transição Energética e Descarbonização
    • Cadeia de fornecimento responsável
  • Operações
    • OPERAÇÕES CIRCULARES E EFICIENTES
    • Ecoeficiência e gestão de resíduos e emissões
    • Carbono Neutro nas Operações
  • Pessoas
    • COLABORADORES E COMUNIDADES ENGAJADOS
    • Crescimento Sustentável das Comunidades
    • Bem-estar Integral, Diversidade e Inclusão
  • Governança
    • GOVERNANÇA E CONDUTA ÉTICA
    • Engajamento e Comunicação Transparente
    • Compliance e Integridade
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

Through the company's strategic direction for its business model, WEG has, in all its business units, more efficient solutions and products with less environmental impact, such as renewable energy (solar and wind power), electric mobility and energy efficiency. WEG develops products considering strict risk criteria related to health and safety. In the development phase, analyzes such as Quality Function Deployment (QFD) and Risk Assessment are applied.

Below are some highlights, considering the variety of products and solutions that the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solar Power

WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.

Generación Hidroeléctrica

WEG fue seleccionada para suministrar los generadores de UHE São Roque, situada en Vargem/SC. Los generadores son una de las partes más importantes que componen el emprendimiento de UHE São Roque. Con 285 toneladas cada uno, y aproximadamente ocho metros de diámetro, estos equipos están entre los hidrogeneradores eléctricos más grandes producidos por WEG.

UHE São Roque tiene potencia instalada de 142 MW que, en promedio, es suficiente para abastecer una ciudad con aproximadamente 170 mil habitantes. Los generadores entraron en operación comercial en julio de 2022.

Almacenamiento de Energía Comercial e Industrial

Los sistemas de almacenamiento de energía son utilizados en instalaciones comerciales o industriales, siendo la solución completa para almacenamiento y gestión de energía eléctrica almacenada, pudiendo ser configurados para desempeñar varias funciones en sistemas inteligentes de generación, transmisión y distribución de energía eléctrica. El sistema está compuesto por una solución de control y gestión energética, siendo indicado principalmente para aplicaciones en sistemas instalados detrás del medidor en industrias, comercios, shopping centers, condominios residenciales e infraestructuras de movilidad eléctrica.

Transformadores para Energías Renovables

La confiabilidad de los transformadores desarrollados para centrales solares tiene como objetivo la garantía del suministro de energía, permitiendo acceso a electricidad por medio de fuentes de generación de energía renovable. En la línea de transformadores para centrales eólicas, WEG desarrolló el proyecto eléctrico y mecánico del transformador extremadamente compacto. Adicionalmente, por la configuración de la instalación, en la cual la fuente y la unidad transformadora se encuentran muy cerca entre sí, el sistema posibilita menos pérdidas y más eficiencia energética.

Movilidad Eléctrica

Soluciones integradas para vehículos eléctricos

WEG desarrolla continuamente tecnologías innovadoras para crear sistemas de tracción eléctrica, así como toda la infraestructura eléctrica necesaria para operación de vehículos eléctricos. Los sistemas de tracción eléctrica WEG pueden ser aplicados en diversos vehículos carreteros, ferroviarios y de navegación, tales como camiones y ómnibus urbanos, furgones, apiladoras eléctricas, trenes, monorrieles, barcos de soporte y remolcadores.

Soluciones digitales

Sistemas inteligentes y sustentables

Los sistemas inteligentes son capaces de integrar los más variados dispositivos y máquinas, así como instalaciones y procesos, promoviendo eficiencia en la toma de decisión y aumento de la eficiencia operacional. Soluciones y sistemas más inteligentes también promueven la utilización más eficiente de recursos energéticos, ayudando a reducir la huella de carbono de las operaciones, en todos los niveles.

Sistemas de Automatización

WEG suministra sistemas de control completamente integrados, garantizando también alto desempeño de los procesos industriales, facilidad de operación y ganancia de productividad, por medio de tecnología de punta. El éxito de la integración de este sistema está en la sinergia de los productos WEG, en la cual motores, drives, generadores, tableros eléctricos y software son integrados, suministrando la solución ideal para cada necesidad. El control de procesos industriales exige sistemas de automatización con elevado grado de confiabilidad y disponibilidad, además de facilidad para equipos de mantenimiento en la gestión de activos, extendiendo la vida de los equipos y racionalizando el uso de recursos.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

WEG Transformer Fleet Management es la solución ideal para monitorear online y supervisar la flota de transformadores a aceite o del tipo seco, posibilitando que los clientes maximicen la eficiencia de sus operaciones, en apoyo a la gestión optimizada de plantas industriales, de generación de energías renovables y de infraestructura. Por otro lado, la solución WEG Power Transformer Specialist es una solución digital aplicada en el monitoreo y en la gestión de transformadores de potencia que, integrada a la plataforma WEG Transformer Fleet Management, centraliza las señales de una serie de sensores instalados en el equipo.

WEG Motion Fleet Management

Desarrollado para llevar más practicidad y agilidad a la operación, en el mantenimiento y en la gestión de plantas industriales, el WEG Motion Fleet Management es la solución ideal para monitorear y elevar la disponibilidad de la flota de accionamiento industrial. Basado en tecnología “cloud computing”, el monitoreo de los activos puede ser seguido en cualquier momento y desde cualquier parte del mundo. Con el Motion Fleet Management es posible conocer el estado operacional de motores y drives (convertidores y arrancadores suaves) de baja y media tensión, reductores, motorreductores, compresores, entre otros activos que estén aplicados en cualquier tipo de industria o instalación

Tecnología Ultra Low Bake (ULB) para Pinturas

La tecnología Ultra Low Bake (ULB) consiste en reducir el tiempo de cura o la temperatura de cura de las pinturas en polvo. Asociado a esa reducción de tiempo o temperatura (que puede llegar a 35% de reducción), reduciendo la cantidad de gas que es utilizada en los hornos de cura de sus clientes y aliados, así como reduciendo las emisiones de GEE.

Los aliados de WEG que poseen esa tecnología en su línea de producción, además de la reducción del impacto ambiental, tienen aumento significativo de productividad y en su competitividad. WEG cuanta con cuarenta productos desarrollados con esa finalidad.

Eficiencia material y evaluación ambiental del producto

WEG adopta, en su cadena de valor, iniciativas que están alineadas a los principios de la economía circular, a través de prácticas como reinserción de residuos de los procesos como materias primas, como por ejemplo chatarra de acero de la estampería, para fabricación de piezas fundidas, adopción de programas de recuperación de materiales en el fin del ciclo de vida de productos, a través de la logística reversa y de planes de cambio.

La aplicación de esos conceptos y prácticas permitieron a WEG alcanzar un índice de eficiencia material de cerca de 85%. WEG también está en constante mejora y evolución de la eficiencia energética de sus productos y de soluciones de retrofit para la extensión de la vida útil de algunas líneas de productos. Equipos cualificados actúan tanto en los procesos de desarrollo de nuevos productos y en la concepción de nuevas líneas, como en la implantación de procesos industriales más eficientes.

WEG aplica el ACV (Análisis de Ciclo de Vida), generando los EPDs (Environmental Product Declarations) conforme las demandas de los clientes, con el objetivo, en los próximos años, de ampliar la aplicación de esas herramientas.

Sepa más sobre las acciones de WEG en Sustentabilidad

Hotel & SPA frente al mar en el noreste de Brasil será alimentado por transformador encapsulado en seco de WEG

Hotel & SPA frente al mar en el noreste de Brasil será alimentado por transformador encapsulado en seco de WEG

Reconocido por su eficiencia energética y confiabilidad, el transformador seco es la opción ideal para aplicaciones en el segmento de infraestructura

WEG publica su Informe Anual Integrado, reforzando su compromiso con la sostenibilidad

WEG publica su Informe Anual Integrado, reforzando su compromiso con la sostenibilidad

La compañía presenta avances significativos en diversas áreas

WEG suministra hidrogeneradores para proyecto en Portugal

WEG suministra hidrogeneradores para proyecto en Portugal

Los hidrogeneradores fortalecerán la producción de energía renovable en la central hidroeléctrica

WEG impulsa el Proyecto Sucuriú, la primera fábrica de celulosa blanqueada de Arauco en Brasil

WEG impulsa el Proyecto Sucuriú, la primera fábrica de celulosa blanqueada de Arauco en Brasil

Soluciones tecnológicas de WEG refuerzan la eficiencia, confiabilidad y sostenibilidad en el sector de celulosa

WEG alcanza los dos mil generadores suministrados al cliente Vestas en Brasil

WEG alcanza los dos mil generadores suministrados al cliente Vestas en Brasil

Un hito que refuerza la sólida alianza y el compromiso con las energías renovables

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Teléfono: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability