WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

Through the company's strategic direction for its business model, WEG has, in all its business units, more efficient solutions and products with less environmental impact, such as renewable energy (solar and wind power), electric mobility and energy efficiency. WEG develops products considering strict risk criteria related to health and safety. In the development phase, analyzes such as Quality Function Deployment (QFD) and Risk Assessment are applied.

Below are some highlights, considering the variety of products and solutions that the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solarenergie

Die WEG festigt sich als einer der führenden Anbieter von Produkten und Lösungen für Solarkraftwerke in Brasilien und bringt die Effizienz, die die Nachhaltigkeit in Städten, Industrien, der Landwirtschaft und den Häusern im ganzen Land vorantreibt. Die WEG verfügt über ein umfangreiches Portfolio an Produkten für Photovoltaik-Projekte in allen Phasen des Unternehmens, mit Lösungen für das Energiewandlungssystem und die interne Verteilung der Anlage bis zum Anschlusspunkt an das Stromnetz über Hochspannungssubstationen.

Production hydroélectrique

WEG a été sélectionnée pour fournir les générateurs de l'UHE São Roque, située à Vargem/SC. Les générateurs sont l'une des parties les plus importantes qui composent le projet pour l'UHE São Roque. Pesant 285 tonnes chacun et ayant un diamètre d'environ huit mètres, ces équipements sont parmi les plus grands hydrogénérateurs électriques jamais produits par WEG.

L'UHE São Roque a une puissance installée de 142 MW qui, en moyenne, est suffisante pour alimenter une ville d'environ 170 000 habitants. Les générateurs sont entrés en service commercial en juillet 2022.

Stockage d'énergie commerciale et industrielle

Les systèmes de stockage d'énergie sont utilisés dans les installations commerciales ou industrielles, offrant une solution complète pour le stockage et la gestion de l'énergie électrique stockée, pouvant être configurés pour exercer plusieurs fonctions dans des systèmes intelligents de génération, de transmission et de distribution d'énergie électrique. Le système est composé d'une solution de contrôle et de gestion énergétique, étant principalement indiqué pour des applications dans des systèmes installés derrière le compteur dans les industries, les commerces, les centres commerciaux, les condominiums résidentiels et l'infrastructure de mobilité électrique.

Transformateurs pour Énergies Renouvelables

La fiabilité des transformateurs développés pour les centrales solaires vise à garantir l'approvisionnement en énergie, permettant l'accès à l'électricité par le biais de sources de production d'énergie renouvelable. Dans la gamme de transformateurs pour les centrales éoliennes, WEG a développé un projet électrique et mécanique pour un transformateur extrêmement compact. En outre, en raison de la configuration de l'installation, où la source et l'unité de transformation sont très proches l'une de l'autre, le système permet moins de pertes et plus d'efficacité énergétique.

Mobilité Électrique

Solutions intégrées pour véhicules électriques

WEG développe constamment des technologies innovantes pour créer des systèmes de traction électrique, ainsi que toute l'infrastructure électrique nécessaire pour le fonctionnement des véhicules électriques. Les systèmes de traction électrique WEG peuvent être appliqués à divers véhicules routiers, ferroviaires et de navigation, tels que les camions et les bus urbains, les fourgonnettes, les chariots élévateurs électriques, les trains, les monorails, les navires de soutien et les remorqueurs.

Solutions Numériques

Systèmes intelligents et durables Les systèmes intelligents sont capables d'intégrer les dispositifs et les machines les plus variés, ainsi que les installations et les processus, favorisant l'efficacité dans la prise de décision et l'augmentation de l'efficacité opérationnelle. Des solutions et systèmes plus intelligents favorisent également une utilisation plus efficace des ressources énergétiques, aidant à réduire l'empreinte carbone des opérations à tous les niveaux.

Automation Systems

WEG supplies completely integrated control systems that guarantee high performance of industrial processes, easy operation and productivity gains by means of state-of-the-art technology. The success of the integration of this system is in the synergy of WEG products, where motors, drives, generators, electric panels and software applications are integrated, providing the ideal solution for each requirement. The control of industrial processes requires automation systems with high reliability and uptime levels, in addition to easy asset management by the maintenance teams, extending the equipment service life and streamlining the use of resources.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

WEG Transformer Fleet Management is the ideal solution to monitor online and manage the fleet of oil or dry-type transformers, enabling customers to maximize the efficiency of their operations, supporting the streamlined management of industrial plants, renewable energy generation and infrastructure. WEG Power Transformer Specialist is a digital solution used to monitor and manage power transformers that, integrated with the WEG Transformer Fleet Management platform, centralizes the signals from several sensors installed on the equipment.

WEG Motion Fleet Management

Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.

Ultra Low Bake (ULB) Technology for Coatings

The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.

WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.

Eficiencia material y evaluación ambiental del producto

WEG adopta, en su cadena de valor, iniciativas que están alineadas a los principios de la economía circular, a través de prácticas como reinserción de residuos de los procesos como materias primas, como por ejemplo chatarra de acero de la estampería, para fabricación de piezas fundidas, adopción de programas de recuperación de materiales en el fin del ciclo de vida de productos, a través de la logística reversa y de planes de cambio.

La aplicación de esos conceptos y prácticas permitieron a WEG alcanzar un índice de eficiencia material de cerca de 85%. WEG también está en constante mejora y evolución de la eficiencia energética de sus productos y de soluciones de retrofit para la extensión de la vida útil de algunas líneas de productos. Equipos cualificados actúan tanto en los procesos de desarrollo de nuevos productos y en la concepción de nuevas líneas, como en la implantación de procesos industriales más eficientes.

WEG aplica el ACV (Análisis de Ciclo de Vida), generando los EPDs (Environmental Product Declarations) conforme las demandas de los clientes, con el objetivo, en los próximos años, de ampliar la aplicación de esas herramientas.

En savoir plus sur nos actions en durabilité

Seaside Hotel & SPA in Northeastern Brazil to Be Powered by WEG Encapsulated Dry-Type Transformer

Seaside Hotel & SPA in Northeastern Brazil to Be Powered by WEG Encapsulated Dry-Type Transformer

Renowned for its energy efficiency and reliability, the dry-type transformer is the ideal choice for infrastructure applications

WEG releases Integrated Annual Report, reinforcing its commitment to sustainability

WEG releases Integrated Annual Report, reinforcing its commitment to sustainability

Company reports significant progress across multiple areas

WEG supplies hydrogenerators for project in Portugal

WEG supplies hydrogenerators for project in Portugal

The hydrogenerators will strengthen renewable energy production at the hydroelectric power plant

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG's technological solutions enhance efficiency, reliability, and sustainability in the pulp sector

WEG reaches two thousand generators supplied to Vestas in Brazil

WEG reaches two thousand generators supplied to Vestas in Brazil

A milestone that reinforces a strong partnership and commitment to renewable energy

Groupe WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Téléphone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability