Por medio del direccionamiento estratégico de la compañía para su modelo de negocio, WEG tiene, en todas sus unidades de negocio, soluciones y productos más eficientes y con menor impacto ambiental, como energías renovables (solar, eólica), movilidad eléctrica, eficiencia energética, entre otras. WEG desarrolla productos considerando estrictos criterios de riesgo relacionados con la salud y la seguridad. En la fase de desarrollo se aplican análisis como el Despliegue de la Función de Calidad (QFD) y la Evaluación de Riesgos.
A seguir son presentados algunos destaques, considerando la variedad de productos y soluciones que la empresa suministra al mercado, por medio de sus diferentes unidades de negocios.
Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.
High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.
For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.
In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.
WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.
WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.
São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.
Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.
The reliability of the transformers developed for solar plants aims at guaranteeing the supply of energy, allowing access to electricity through renewable energy generation sources. In the line of transformers for wind farms, WEG developed an extremely compact electrical and mechanical transformer design. Additionally, due to the installation layout, in which the source and the transforming unit are very close to each other, the system produces smaller losses and greater energy efficiency.
WEG desarrolla continuamente tecnologías innovadoras para crear sistemas de tracción eléctrica, así como toda la infraestructura eléctrica necesaria para operación de vehículos eléctricos. Los sistemas de tracción eléctrica WEG pueden ser aplicados en diversos vehículos carreteros, ferroviarios y de navegación, tales como camiones y ómnibus urbanos, furgones, apiladoras eléctricas, trenes, monorrieles, barcos de soporte y remolcadores.
Los sistemas inteligentes son capaces de integrar los más variados dispositivos y máquinas, así como instalaciones y procesos, promoviendo eficiencia en la toma de decisión y aumento de la eficiencia operacional. Soluciones y sistemas más inteligentes también promueven la utilización más eficiente de recursos energéticos, ayudando a reducir la huella de carbono de las operaciones, en todos los niveles.
WEG suministra sistemas de control completamente integrados, garantizando también alto desempeño de los procesos industriales, facilidad de operación y ganancia de productividad, por medio de tecnología de punta. El éxito de la integración de este sistema está en la sinergia de los productos WEG, en la cual motores, drives, generadores, tableros eléctricos y software son integrados, suministrando la solución ideal para cada necesidad. El control de procesos industriales exige sistemas de automatización con elevado grado de confiabilidad y disponibilidad, además de facilidad para equipos de mantenimiento en la gestión de activos, extendiendo la vida de los equipos y racionalizando el uso de recursos.
WEG Transformer Fleet Management es la solución ideal para monitorear online y supervisar la flota de transformadores a aceite o del tipo seco, posibilitando que los clientes maximicen la eficiencia de sus operaciones, en apoyo a la gestión optimizada de plantas industriales, de generación de energías renovables y de infraestructura. Por otro lado, la solución WEG Power Transformer Specialist es una solución digital aplicada en el monitoreo y en la gestión de transformadores de potencia que, integrada a la plataforma WEG Transformer Fleet Management, centraliza las señales de una serie de sensores instalados en el equipo.
Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.
The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.
WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.In its value chain, WEG adopts initiatives in line with the principles of the circular economy, using practices that include the reuse of process residues as raw material, like stamping steel scrap used to make castings, and the adoption of programs to recover materials at the end of the product life cycle through reverse logistics and replacement plans.
The application of these concepts and practices allowed WEG to achieve a material efficiency rate close to 85%. WEG is also constantly improving and evolving the energy efficiency of its products and retrofit solutions to extend the service life of some product lines. Qualified teams work on the processes to develop new products, on the design of new lines and in the implementation of more efficient industrial processes.
WEG applies the LCA (Life Cycle Analysis) to generate the EPD (Environmental Product Declarations) according to the customers’ demands, intending, in the coming years, to expand the application of these tools.